CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service
Description
CIMPLICITY Configuration Microservice exposes a set of APIs that enable you to configure a CIMPLICITY project. The base URL is https://localhost:9443/cim-config/v1
All Operations
Get/projects/{projectId}
returns the project name for the given project id
Get/projects/{projectId}/classes
returns the list of classes in a project
Get/projects/{projectId}/devices
returns an array of devices in the project optionally filtered by port prefix
Get/projects/{projectId}/historianConnections
returns a list of historianConnections in a project that satisfy the filter criteria
Post/projects/{projectId}/historianConnections
Creates or updates an array of historian connections in the project
Post/Projects/{projectId}/historianConnections:batchDelete
Deletes an array of historain connections in the project
Post/projects/{projectId}/historianConnections:read
Gets an array of historian connection objects that satisfy the filter criteria specified in the request body.
Get/projects/{projectId}/objects
returns a list of objects in a project that satisfy the filter criteria
Post/projects/{projectId}/objects
Creates or updates an array of objects in the project
Post/Projects/{projectId}/objects:batchDelete
Deletes an array of objects in the project
Post/projects/{projectId}/objects:read
Gets an array of class Objects that satisfy the filter criteria specified in the request body.
Post/projects/{projectId}/operationsHub-settings
Add or individually modify parameters related to Operations Hub
Get/projects/{projectId}/points
Gets an array of point objects that satisfy the query criteria
Post/projects/{projectId}/points
Creates or updates an array of points in the project
Post/Projects/{projectId}/points:batchDelete
Deletes an array of points in the project
Post/projects/{projectId}/points:read
Gets an array of point objects that satisfy the filter criteria specified in the request body.
Get/projects/{projectId}/resources
returns a list of resources in a project that satisfy the filter criteria
Post/projects/{projectId}/resources
Creates or updates an array of resources in the project
Post/Projects/{projectId}/resources:batchDelete
Deletes an array of resources in the project
Post/projects/{projectId}/resources:read
Gets an array of resource objects that satisfy the filter criteria specified in the request body.
Get/projects/{projectId}/roles
returns a list of roles in a project that satisfy the filter criteria
Post/projects/{projectId}/roles
Creates or updates an array of roles in the project
Post/Projects/{projectId}/roles:batchDelete
Deletes an array of roles in the project
Post/projects/{projectId}/roles:read
Gets an array of role objects that satisfy the filter criteria specified in the request body.
Get/Projects/{projectId}/runningStatus
returns a running status of the CIMPLICITY project
Post/Projects/{projectId}/runningStatus
start or stop a CIMPLICITY project
Post/Projects/{projectId}/runningStatus:read
Deletes an array of objects in the project
Get/projects/{projectId}/SQLConnections
Gets an array of SQL connections objects that satisfy the query criteria
Post/projects/{projectId}/SQLConnections
Creates or updates an array of sql connections in the project
Post/projects/{projectId}/SQLConnections:read
Gets an array of SQL Connections that satisfy the filter criteria specified in the request body.
Get/projects/{projectId}/users
returns a list of users in a project that satisfy the filter criteria
Post/projects/{projectId}/users
Creates or updates an array of users in the project
Post/Projects/{projectId}/users:batchDelete
Deletes an array of users in the project
Post/projects/{projectId}/users:read
Gets an array of users objects that satisfy the filter criteria specified in the request body.
Post/rest-settings
modifies rest settings of multiple projects
Get/service-settings
returns settings that can be used by the client
Post/user-config
creates or modifies a user
Json Schemas
Fields that describe the connection to a SQL connection
Fields that describe the connection to a SQL connection
Fields that need to be specfied for creating a user before enabling rest configuration for project
Fields that need to be specfied for modifying rest settings of project
Fields that describe the connection to a historian server
Fields that describe the resource
Fields that describe the user
Fields that describe the role
Contains the previliges related to security
Contains the previliges related to configuration security
Fields that describe the context for referencing an OPC UA Devices NodeIds
is an object that represents an attribute of an object.
is an object that represents a dataitem of an object.
is an object that describe a CIMPLICITY class object instance
fields that describe a CIMPLICITY point
Contains the properties pertaining to Derived Point Configuration
object contains the device information for a CIMPLICITY point.
object contains the conversion information for converting a point from raw device units to real-world units. Conversion can either be linear or based on a conversion expression
is a object to configure the expression attributes
Represents measurement unit.
Represents a point enum that contains a list of point enum fields.
Represents a point enum field that associates a text string with an integer point value.
object contains the point alarm information for a CIMPLICITY point
object provides an interface to CIMPLICITY Alarm configuration
object contains the trend point buffering information for a CIMPLICITY point
result information about each item in a create/update/delete request
 
 
 
 
Specifies calculation types of points
Specifies initial value for a global or derived point.
MMS types
defines the trigger condition for a device point. See the Point Configuration documentation for additional information
defines update criterias available for device points. The particular types of update that are actually available depend on the device communication module being used
Specifies the browser type
defines different change approval data setting. The numeric value of these enumerations can be used in an expression of a class data item for the $APPROVAL_TYPE field
defines the deletion options available for an alarm
defines types of alarming available
defines the orgin types for a point
defines units for time values
Response data when a request fails
The results of the create/update/delete operations.
The results of the point create/update/delete operations.
The results of the points get query
The results of the points get query.
The results of the historian connections get query.
The results of the resources get query.
The results of the roles get query.
The results of the objects get query
The results of the users get query.
The running status of the CIMPLICITY project.
The results of the Settings Get.
Information about the CIMPLICITY project
CIMPLICITY class definition
CIMPLICITY class definition
A data item in a class (becomes a point on an object)
one child composite member of the class
Filter used for objects
Filter used for SQL connections
An object which provides an interface for filters to read point configuration
An object which provides an interface for filters to read historian connections configuration
An object which provides an interface for filters to read resources
An object which provides an interface for filters to read roles
An object which provides an interface for filters to read users